This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C2000 coding using simulink



I;m working on f28027 micro-controller and trying to code it using simulink.........First I tried to configure an ADC in Simulink  and build it, the code runs fine on c2000 but the changes are not made in the real time in the ADC output, only after stopping the changes are made in the memory blks......aslo I want to compare 2 ADC signals, for that which simulink blk should I use?????.........I want to multiply 2 ADC signals too....I want to multiply ADC with a constant blk to read the measured values, so how I have to configure the constant block to match the data types and multiply........Please help me out in this, Its urgent......Is there anyone I can contact and can help me out in this?