Other Parts Discussed in Thread: TMS320F28377S
hi !
we are using the LAUNCHXL-F28377S and the IDDK code example, and now we want do design our own pcb board with the delfino TMS320F28377S.
the are 3 switches in the above mentioned launchpad , one for JTAG_TRST , and 2 for GPIO 84 and GPIO 72.
as i understand it , if i want to run my application in stand alone (boot from flash) mode , i need to tie both GPIOs to "High" , but what if i want to connect external emulator like the XDS100v2? ,do i have to add a TRST switch like in the launchpad? , i don't fully understand this issue , doesn't the emulator supposed to control the TRST signal?
another question is realtaed to the boot loader - if i order a TMS320F28377S chip , do i need to upload a boot loader?
best regards
MARK