This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

3ph Motor - FOC Sensored/sensorless used with C2000 (F28M35H51C)

Hi at all,
I have a basic Question. Is possible to run a 3Ph motor controlled by F28M35.
I try to use the FOC code (controleSUITE - Development Tools - Motor - Example Project - ACI FOC Sensored or Sensorless) in my Project.
I have copied the header files from the Sensored Project into my Project and add the References to the Header-Files to the Compiler Include Options.
But there are some Header-Files for the f2803 and I can't finde the corresponding files for F28M35.
Resulting by this missing Files, I got a mass of errors.

Is there a way to integrate the sensored or sensorless FOC functionality into my Project, to run a 3ph motor?