This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CLA and DCSM

Hi there,

I have been trying the CLA with Example_2805xClaAdc on a F28055 and have found that CLA isn't running at all; it will not stop at the break point I set at CLA ISR, nor the variable, ConversionCount, will increase and then reset.  However, when I try the same sample code on a brand new board, everything works fine.  These two boards are identical, but I previously enabled DCSM on the old board.  Does DCSM has anything to do with CLA not running?  If so, how can I get CLA to work on the device whose DCSM was once enabled?

Thank you

regards,

Kevin