Other Parts Discussed in Thread: CONTROLSUITE
I am using F28069 Control Stick in which i am trying to catch the sin wave from the funtion generator. I am running ContinuousADC program to acquire the analog signal that is coming from the function generator. There are 3 things that i want to ask.
1) When i am giving the input with the signal generator through the probe it is not acquiring the signal. I am giving input to the pin2 and grounding with pin 32. But when i give the input without probe directly toughing the jumper wires with channel it is showing variation. Why?
Is this is happening because the probe is not compatible with the piccolo and piccolo is not able to detect the signal.?
2) Major problem.. Even when is am toughing the jumper wire with the input and it is changing it is not able to detect the signal with high frequency I am not able to configure why this happening. It is able to project 2-3 values/ second. I am totally new with the micro-controller from last 2 months i am trying to catch this signal but for no avail.
3) There is CLA circuit also present in this micro-controller should i use that to plot the graph with more accuracy in the GUI. BUt there is a problem i donot knw how to use that neither the programming. :(