This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Applying SPWM scheme for Induction Motor with C2000F28027F launchpad + BOOSTXL-DRV8305EVM

Other Parts Discussed in Thread: DRV8301, BOOSTXL-DRV8305EVM, MOTORWARE

Hello sir,

I have following harware

(1) C2000F28027 and C2000F28027F launchpad

(2)Boostxl DRV8301_(24 V )  boosterpack and  BOOSTXL-DRV8305EVM_(48 V)

I have demostrated instaspin FOC in BLDC motor with (c2000f28027F+Boostxl DRV8301) combination.

but my next project is to apply SPWM  scheme to the Induction Motor.

AS in case of Instaspin FOC we  have refference project code in Motorware software  ( Project Lab_5[b] ), like that can we get the refference code in the control suit software for SPWM scheme.

can we use {{ DRV 8305 EVM board in conjuction with C2000f28027F }} for applying SPWM scheme for induction motor.

please tell me which code example i have to used from the control suit for this SPWM scheme.

  • what do you mean by SPWM?

    we use an SVPWM technique, with modulation options that allow you to limit to pure sinewave, space vector modulation, and full trapezoidal over-modulation.

    you can run induction motors with IS-FOC

    LVACIMTR is an example of one that will run with your hardware