Other Parts Discussed in Thread: TMS320F28PLC84, AFE031
Hi
I have just started working on a project that involves Power line communication, main requirements are
Power line voltage 600V, 50/60 Hz, if possible also 400Hz.
This high voltage supply line is not connected to power distribution so violating any allocated frequency band is not an issue.
Distance between terminal is 3km, bit more is required for head room
Ideally modulation scheme is BELL 202 standard (FSK 1200/2200Hz Mark/space) or as close as possible in terms of frequency modulation and baud rate.
I have looked around but was unable to find something in that low frequency range. The lowest and nearest I can see is TMS320F28PLC84 + AFE031 reference design but it is recommended for 35kHz to 90 kHz frequency range.
If anyone can suggested reference design that need minimum changes.
Thanks in advance
M Mujahid