Other Parts Discussed in Thread: CONTROLSUITE
Hi
I am a beginner with the TI microcontrollers. I felt it would be really useful to start learning the TI set of microcontrollers as well. A friend suggested me to start with the C2000 set of microcontrollers as I have the Piccolo F28069 controlSTICK with me. This I believe is a development kit making use of C2000 controller. I installed the CCS (ver 6.1.2) and the control suite 3.3.9. I also went through Lab1 of of student workshop which I got from your forum.
Could someone tell me as to how I should go about when I start writing my own code. In the lab1 document i saw there was a main file, an include file with a lot of sub files and a linker file. (This was a program to find the sum of two numbers). While writing my own code what should I do with the linker file and include files? Are these two automatically generated?
Is there any good video tutorial that I might get to get started with this set of controllers?
Is there any additional material that I get on Piccolo F28069 controlSTICK?
Hope my questions are not too vague.I am finding it a bit confusing since MPLAB (which I am familiar with) is completely different from code composer studio.
Thank you
Hari