Other Parts Discussed in Thread: DRV8301, INSTASPIN-BLDC, CCSTUDIO
Hi,
I need to design a drive for a 5kW sensorless BLDC motor rated at 180V. All the development kits I have come across are rated at 60V. (e.g. http://www.ti.com/tool/drv8302-hc-c2-kit)
Please suggest how I can use the kit's control output signals to drive external 3 phase bridge built using IGBTs rated at 75A, 600V. Do I need to modify the current sensing scheme as well?
Any alternatives other than the DRV8302-HC-C2 kit?
Thanks,
Jayant