Hi,
I am trying to power a F28027 launchpad in stand alone mode. How do I start the code once I power it on? Or how do I know the code is programmed on the launch pad? I built it through CCS and then unplugged it and took off JP1, JP2, and JP3 and then powered it on with 3.3V but it doesn't appear to run my code. I am very unfamiliar with microcontrollers and would really appreciate the help. I attempting looking through user guides and other forums but could not find the solution. Thank you!