This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8312EVM with CC2803x

Other Parts Discussed in Thread: CONTROLSUITE

Dear all.

I have the TI DRV8312EVM Rev.D kit and CC2803x iso dimm.

I have programmed the InstaSPIN-BLDC_GUI_DRV8312_v104.out firmware and used the related application .

My motor have 1 pole pair, and in the setting TAB it isn't possible to select a 2 pole.

Anyway with InstaSPIN-BLDC_GUI_DRV83xx_v104.exe, I'm able to drive the motor up to a speed of approximately 30k rpm (displayed 15k )

How can I test the motor wih 2 pole and 40k rpm ?

How can I find the file source of InstaSPIN-BLDC_GUI_DRV8312_v104.out firmware ?

Thanks

  • GUI project source is here
    C:\ti\controlSUITE\development_kits\DRV8312-C2-KIT_v128\GUI_project_InstaSPIN_BLDC

    but if you rebuild it will only work with the GUI if all the variables stay in the exact same location. or just use this project to w/o the GUI and run from CCS.

    you can also just start with the baseline build level project
    C:\ti\controlSUITE\development_kits\DRV8312-C2-KIT_v128\InstaSPIN_BLDC