Other Parts Discussed in Thread: TMS320F28027F, TMDSHVMTRINSPIN
Hello,
I'm using instaspin with TMS320F28027F microcontroller. I use my own hardware design. After identifying my induction motor i used lab5b. Everything is well until the stator frequency goes under 4Hz. At this time the stator current goes up to the value defined by USER_MOTOR_MAX_CURRENT. The motor has no load. So the current musn't be so high under 4Hz. What may cause this high current.