This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Naming / Aliasing GPIO pins

Other Parts Discussed in Thread: TMS320F28335

I am working on code for a TMS320F28335 in Code Composer Studio 6.1.2.00015

I would like to create meaningful aliases for my GPIO pins (ADC_chipselect, LED0, etc.), but I am having trouble coming up with the right way to do it.

I have tried this:

Uint16 *LED0;
LED0 = &GpioDataRegs.GPADAT.bit.GPIO16

but the compiler tells me I can't get the address of a bit field. Aliasing, 32 bits at once is not really going to help me. Can someone point me in the right direction?

Thank you!

   Daniel

 

  • Daniel,

    I guess you could just define each bitfield of interest as some meaningful name and then use it in your code, like this:

    #define LED                      GpioDataRegs.GPBDAT.bit.GPIO34
    #define LEDTOGGLE     GpioDataRegs.GPBTOGGLE.bit.GPIO34

    Uint16 var;

    LEDTOGGLE = 1;

    var = LED;

    Any use?

    Regards,

    Richard

  • I am pretty certain that you can just #define the statements. For Example:

    #define LED0_TOGGLE GpioDataRegs.GPBTOGGLE.bit.GPIO34 = 1
    #define LED0_SET GpioDataRegs.GPBSET.bit.GPIO34 = 1
    #define LED0_CLEAR GpioDataRegs.GPBCLEAR.bit.GPIO34 = 1


    Then, in your code you can just do:

    LED0_TOGGLE; // Toggle LED0
    or
    LED0_CLEAR; // Clear LED0

    -Mark