Other Parts Discussed in Thread: CONTROLSUITE
Hi there,
I'm using the eZdsp F28335 and the example project ecap_capture_pwm from the controlSUITE collection (device_support\f2833x\v133\DSP2833x_examples_ccsv4\ecap_capture_pwm).
My problem is that I don't see the PWM on GPIO4 (pin13 on connector P8) and consequently the ECap interrupt is not generated. More specifically, The PWM signal is always at high level if I connect GPIO4 to the Ecap pin, GPIO24 (pin 33 on connector 33), while it is always at low level if cut the connection between the two pins. I'm using pin 39 on connector P8 as ground, but nothing changes if I use any of the other GNDs defined on the eZdsp datasheet.
I was wondering if I missed something configuring the HW (switches, jumpers and so on), or if there is a known issue about this example. For the HW configuration, SW1 is set for jump to SARAM, and actually the code runs, I can debug it; all the JP# are in the same position as shipped from factory.
I don't know if it can be a useful information, but I'm using the XDS200 as JTAG connector.
I thank you in advance for your support,
Filippo