This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Debug Configuration for dual core just by clicking on the bug



Hi,


I'm already working for a while with the F28C36x Concerto Processor which has 2 cores inside. I'm already used to a starting of the debugging session and I'm wondering if there is some quicker possibility.

At the moment it's not very userfriendly, to connect to one core load the program by selecting the correct file. Then connect to the second core and select a different file...

I simply want to click on the Bug-Button to start a debugging session with both cores, so it should automatically connect to both cores and also load the defined programs from both cores.
I hope there is a way via a script or so, because the GUI is obviously only designed for a single core Debugging session.

kind regards

Andy