Other Parts Discussed in Thread: TMS320F28335
6.8 of the TMS320F28335 datasheet gives power sequencing requirements. One of the requirements is that "Vddio and Vdda should always be within 0.3V of each other."
My design uses separate power rails for Vddio and Vdda. Vddio is regulated by a switching regulator. Vdda is regulated by an LDO (some signal conditioning circuits also use the Vdda supply, and for this reason, the use of the switcher with all of its digital loads to provide the supply was not desired). The incoming power to the regulators is the same. So, during steady state conditions, the supplies are always both 3.3V and meet the requirement of being within 0.3V of each other.
The issue is during power-up and power-down. The rise and fall of the supplies during these conditions are not completely in sync. For example, Vdda leads Vddio slightly on power-up so that for a period of about 9ms, the difference between the two supplies exceeds 0.3V.
Is there any acceptable amount of time that the two supplies can have more than 0.3V of potential difference between them?
Or, if no time under these conditions is acceptable, does TI have any design recommendations for this issue when separate supplies are used?
Thanks in advance for your help.