This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CAN: Import of *.ncd database files

Other Parts Discussed in Thread: CONTROLSUITE

Hello,

I am using the Inverter DRV8301-HC-EVM Rev D together with the control card TMDSCND28069. I've seen that it is possible to use CAN on a frame level. Now I am wondering if it is possible to use a national instruments CAN database file (*.ncd) to describe CAN channels. If so, is there also a library available which enables the utilization of CAN on a channel level?

Kind regards,

Oliver 

  • Oliver,
    We do not provide any .ncd file that goes with our CAN. Some of our devices have Driverlib support to use the CAN on a frame level. I am bit unsure what you are asking. Could you please be more specific?
  • I checked with my colleague in the Software group and she mentioned that support for eCAN is not available in the Driverlib for this device. The driverlib on 28069 is limited to USB, and a few others needed to make the Stellaris USB examples easy to port (Interrupt, SysCtl, UART). (Please see C:\ti\controlSUITE\device_support\f2806x\v150\MWare\driverlib directory). As mentioned in the previous post, we do not have any support files to facilitate the usage of .NCD files for CAN.