Other Parts Discussed in Thread: MOTORWARE
Hello,
I have started the InstaSpin Projects & Labs User's Guide, InstaSPIN-FOC & InstaSPIN-MOTION, with the DRV 8301 kit and TMS320F2802X control card.
I am in Code Composer Studio 6 and have Imported the lab1 through 12 Existing CCS/CCE Projects.
My board is powered off 23V and is connected to my computer by the mini USB given in the kit. The board is seen by my computer as COM4 and the two USB controllers "TI XDS100 Channel A and B" are seen as well
I click proj_Lab01 and click build and there are no errors and the build finishes.
The problem start when i click debug as it will say "unable to launch the debug session. the specified file 'C:\users\E5-474G-53QG\workspace\blink LED\New Target Configuration.ccxml'does not exist in the file system"
whta does it mean??