Hi,
I've tried to run the motor with RPM range about ~20,000 RPM with InstaSPIN-FOC launchpad.
However, the motor couldn't reach 20,000 RPM while another BLDC controller which is not FOC reaches 20,000 without problem.
So, my question is, how can I get my motor run in maximum RPM? Do I have to change any configuration?
Actually, motor size is small (22mm diameter). Kv = 2,000.
-Hyon