I have imported the ADC SOC (Software Driver) from controlsuite and I am assuming this is the right ADC code Example. I used this project on control card experimental kit TMS320F28027. I fed an analogue voltage of 3.2V at ADCIN-A0 (Just under 3.3V accepted by ADC ) and observed the variable ADCRESULT0 with watch variable feature in CCSv6 however I am always getting 0x........0000 0000 in the low bits even when analogue is close to 3.3V. Please advise.