Other Parts Discussed in Thread: LAUNCHXL-F28069M, BOOSTXL-DRV8301
Hello -
I recently purchased the LAUNCHXL-F28069M controller/BOOSTXL-DRV8301 drive. I am using both to control a small BLDC blower (12V, 6A).
I have run through most of the lab examples without problems. Today I was working with Lab5e and decided to re-identify the motor. I set the EnableUserParams to 0 and then set EnableSys and Run_Identify to 1. The system then either miss identified the Ls value (1.33mH vice 133uH) or got stuck in the Rs identify routine. Stuck as in the ISR LED was blinking but no updates/changes were occurring in CCS.
After this occurred and after repeating a couple times, I went back to Lab2a and was able to identify the motor without problems. I was also able to run Lab5e with EnableUserParams set to 1 without issue.
Any suggestions on where I am going wrong? Do I need to do something different since I am using SpinTAC in Lab5e?
Thanks in advance!
Brett