This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

xds220 iso and slow code execution on ram

Hi all,

I'm have two xds220 iso emulator one of them makes code execution slow on ram debug mode. With same hardware and same code other emulator works normally. When i load code to flash both of two emulators work fine. 

Days ago i had a communication problem with the emulator and reinstall its firmware but i made a mistake and load wrong firmware "sd_xds200_firmware_v1005.bin"  (i didnt notice the worning " DO NOT APPLY TO XDS220-ISO. THE ISO VERSION IS JTAG ONLY AND DOES NOT SUPPORT SWD, UART OR CJTAG. IT USES A DIFFERENT CPLD AND PROGRAMMING  WITH xds2xx_xc64_swd.xsvf OR xds2xx_xc64.xsvf MAY HAVE ADVERSE SIDE EFFECTS." and load) and then i load "sd_xds220_iso_firmware_v1005.bin" but now it has slow execution problem. Usb and ethernet connection has the same problem

my test environment ccsV6, ezdsp (my own control card has same problem), xds220 iso.