Other Parts Discussed in Thread: CONTROLSUITE, DESIGNDRIVE
Hey together,
i want to use a Hiperface-encoder with a f28m35x Concerto. I have already a RS485 transceiver which provides a TX, RX, CLK and RW (to switch read/write) wire at the output of the transmitter. In this case i need a UART connection to read and write data from the C2000 of the Concerto to the RS485 transceiver.
Does anyone have an example with the hyperface protocol, which i can use to read the Hiperface encoder by UART?
I found only applications for the Sitara AM4xx, but i didn't find any code examples for hiperface on a C2000.
Thanks!
Regards,
Sebastian