Hi everyone,
I'm using Piccolo TMDSCNCD28069 controlCARD and I want to use it with the analog front-end AFE031 for my power line application (e.g exploiting the PHY_G3_EXAMPLE where there is a packet exchange between the two modules and blinking led).
I have the TMDSPLCKIT-V3 KIT and I saw the datasheet connection between F28069 and AFE031 but I'm not sure about them.
I found these connections:
SCI-RXDA ---> GPIO-28
SCI-TXDA ---> GPIO-29
CLOCK (SPI) ---> GPIO-18
STEA (SPI) ---> GPIO-19
SIMOA (SPI) ----> GPIO-16
SOMIA (SPI) ---> GPIO-17
DAC ---> GPIO-07
SD (Shout down afe) ---> GPIO-12
INTERRUPT ---> GPIO-06
ADC IN ---> A-01
I've also seen tidu237.pdf pag.50 (TI G3 Power Line Communication Developer's Kit Design Guide) which is directly correlated to TMDSPLCKIT-V3 and I found out that other GPIO connections have to be connected too:
GPIO20 McBSP (MDXA) Enabled F28069 AFE031 connection
GPIO21 McBSP (MDRA) Enabled F28069 AFE031 connection
GPIO22 McBSP (MCLKXA) Enabled F28069 AFE031 connection
GPIO23 McBSP (MFSXA) Enabled F28069 AFE031 connection
Ps: I also seen afe031 datasheet and F28069 datasheet details.
Can you please explain me how to connect properly F28069 to AFE031?
I hope for your support,
Best,
Andrea