Hello
I am using currently F28335 and also using ti document 3-level SVPWM (SPRABS6).
Induction Motor(3.3kV) Controlling by Sensorless Vector Control. Our 3-level NPC Inverter's switching frequency (Fsw) is 1.5kHz.
I want decrease the Fsw about 0.8kHz~1kHz. When using Fsw=1kHz then controlling the motor rated frequency at 50~60Hz, the 3-level SVPWM output reference resolution is decreased. There is any method to increase good resolution or high performance 3-level SVPWM output reference? Or how to implement dual interrupt method?
Thanks
Erka