Hi,
I viewed this post(
). However the parameters are different from the parameters I saw in the sample solution. Could anyone tell me which one is correct?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I viewed this post(
). However the parameters are different from the parameters I saw in the sample solution. Could anyone tell me which one is correct?
Hi Chris,
The parameters I found in controlsuite are different. Do I need to change the code before running the motor?
#define RS 0.79 // Stator resistance (ohm)
#define RR 0 // Rotor resistance (ohm)
#define LS 0.0012 // Stator inductance (H)
#define LR 0 // Rotor inductance (H)
#define LM 0 // Magnetizing inductance (H)
#define POLES 8