Hello all you genius people,
I'm trying to read different ADC values from two different channels of ADC-A using Simulink, however, one channel always seems to "copy" the value of the other. I'm using the F28377S Delfino Launchpad with a simple Simulink model: ADC-A1 and ADC-A2 each connected to a display block, 12 bit resolution, with all parameters same for both channels except for the SOC sources. I have a potentiometer connected to each pin. Both the ADCs are outputting the value from one of the potentiometers while the other potentiometer does not seem to have any affect on the ADCs.
a) Is it possible to read different values from different channels of the same ADC?
b) If yes, I'm pretty sure it has something to do with ADC pin muxing but I'm super new to the Launchpad, so is there an easy way to do it through Simulink, or can someone guide me through the process?
Thanks!