Some of the CAN registers in CCS have been defined incorrectly. The registers they point to do not correspond with the memory offset shown in the tech manual.
For example, in the tech manual the offset for the CAN_IF2MSK register is 0x124, but actually in CCS the CAN_IF2DATA shows the contents of offset 0x124. There are a number of them that are messed up, though I'm not exactly sure how many.