Other Parts Discussed in Thread: MOTORWARE
Hi,
I have just purchased the InstaSPIN-FOC High Voltage Kit.
I have a BLDC motor with the following basic:
Rotor Pole Pair = 2
Phase = 3
Max RPM = 15K
I have the following identification using the GUI
R = 2.39R
Ls = 0.0137
Flux = 0.326
Therefore
2.39/0.0137 = 174HZ
0.326 / 2pi / 0.013 = 3.91A max current
I have set:
Estimation Freq = 100
Pole Pairs = 1
Max Current = 5
Max Freq = 1200
The trouble I am now faced with is I can only achieve 10KRPM (Measured), whist the GUI is set at 20KRPM.
I need to know what my next step is to achieve higher RPM.
Do I need to use field weakening or is there some other settings I can use to up the RPM.
Thanks in advance for any suggestions.
Cheers