This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Program will not fit into available memory! Is there a fix?



I'm running an simple Simulink model on a Delfino Launchpad F28377S and I get the following error:

"C:/MATLAB/SupportPackages/R2016a/toolbox/target/supportpackages/tic2000/src/c28377S.cmd", line 81: error:
program will not fit into available memory. run placement with
alignment/blocking fails for section ".esysmem" size 0x400 page 1.
Available memory ranges:
RAMLS5 size: 0x800 unused: 0x39b max hole: 0x39b
error: errors encountered during linking; "../test.out" not built

>> Compilation failure
gmake: *** [../test.out] Error 1

N:\My Documents\MATLAB\Solomon\test_ert_rtw>echo The make command returned an error of 2
The make command returned an error of 2

N:\My Documents\MATLAB\Solomon\test_ert_rtw>An_error_occurred_during_the_call_to_make
'An_error_occurred_during_the_call_to_make' is not recognized as an internal or external command,
operable program or batch file.
### Creating HTML report file test_codegen_rpt.html
### Build procedure for model: 'test' aborted due to an error.
Error(s) encountered while building "test":
### Failed to generate all binary outputs.

This is very surprising as my model is extremely simple, so I was wondering if I was doing something wrong that results in this error. Also, I'm a complete newbie to the TI environment, so if there's a fix, it'd be much appreciated if someone can guide me through it.

Thanks!

Solomon