This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Reuse of Default bootpin after boot.



Hello.

I'm using F28377S on a custom board with CCS6.2.1.

Due to a Hardware to Software department communication problem we are using a default bootpin for a chipselect of an ADC. The other bootpin is tied to high and also the CS line has a pullup. So the software is booting from flash in stand alone mode like wanted. Also the ADC is working after booting has completed.

Can there be any other issue because of reusing default bootpin?

Thanks

BR

Christian