Hi,
I'm using the 28069.
What happens if, for example, I set the one-shot to set low on both A and B, and I set DCA/BEVT1 to set high on A and B, and then both events happen at the same time ?
Which event "wins" ?
In the datasheet, on the trip-zone description chapter, Figure 3-39, it shows that both signals enter "trip logic", but then it is not elaborated further.
Can you please explain what will happen?
Thanks