Helo,
I have a controlCARD F28069MPZT and Driver 8301 Dev. Now, I have implanted my code on Flash of microcontroller. But the problem is when I supplied power for driver, the controlCARD did not run, but if I connect controlCARD through USB in the same time with Driver, it worked and controlled well my motor.
I noticed that at the moment I connect cable USB, 2 leds D2 and D4 blinked and somehow the connection with USB port charged the microcontroller and made it wake up. I think that maybe that there are 3 possibilities :
1 . The connection USB supplies power for FTDI chip and it activated microcontroller
2. Configuration in my code that doesn't allow microcontroller to boot from flash itself after being supplied by Driver
3. Switches configuration for Boot Mode.
But I do not still find out solutions. I wonder if anyone has the same problems before, pls help
Thanks all ur help