This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADC offset shift issue of TMS320F28032PAGT

Other Parts Discussed in Thread: CONTROLSUITE

Will the ADC offset shift when running a few years? Do we have the reliability test data prove it can meet the spec after running a few years? Will we test the ADC offset during our production? Is the test item a go-no-go test or can test the value? Thanks

  • Hi Jeffery,

    In general DS min/max specifications incorporate aging considerations and can thus be trusted to be accurate over the life of the part. We do accelerated aging experiments (i.e. high temperature and supply voltage bake), design simulations, and/or use manufacturing process information as appropriate to determine this.

    This is a bit moot for this particular parameter because we require the customer to perform self-calibration of this parameter each time the device starts up.

    If the customer is particularly sensitive to offset error, they can run periodic offset re-calibration on this device (instead of just at start-up). The ControlSUITE header files provide an example of offset self-calibration that the customer can modify to run periodically. Note that the software provided in ControlSUITE is not a call-and-forget function: the customer must modify it to work with their system!
  • Hi Devin

    Thank you for your quick response. Based on our accelerated aging experiments, could you help to tell me where this parameter will shift and why it will shift? Thanks

    Best Regards
    Jeffery Chen
  • Hi Jefferey,


    This particular parameter is only specified when the customer performs self-calibration at each start-up, so aging will be automatically compensated for.

  • Devin

    One more question, which factors will make this parameter offset worse? For example, the application environment, the life time? Thanks