Hi
1) If I commission one of the G3 PLC kits as a base node (using the older PLC 83 kits) and start a Network.
2) Then I start a service node on another G3 PLC kit and it attaches to the base node started in step 1.
3) Now the base node and service node are able to communicate with each other.
4) I unplug the usb cable from my computer for the g3 plc kit started in Step 1. However, the kit is still powered up and running.
5) Now start a third G3 PLC kit as a service node and allow it to discover and attach to the G3 PLC kit started in step 1.
6) Now attach the usb cable from G3 PLC KIT started in step 1 to my computer.
Question: Are there commands to read the 2 devices attached in steps 2 and step 5 from the base node. During all through this process the G3 PLC kit started in step 1 is always powered on. Since the host has lost communication to the base node in the G3 PLC kit, there is no record of the attach indication to know when a device has joined. Is it possible to read the currently joined nodes from the base node and find their extended addresses.
Kind Regards
Viswanath