This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Migrating from TMS320F28027 to TMS320F28034

Other Parts Discussed in Thread: TMS320F28034, CONTROLSUITE

I have been given a project form another engineer.   The project is build in CCS Version: 6.1.1.00022.  It uses a linker command file called

F28027F.cmd posted below.   Where would the previous engineer get this file?   I would now like to compile the same code for the TMS320F28034.   

How do I migrate?  Is there a F28034F.cmd that I can start with?

/*
// TI File $Revision: /main/7 $
// Checkin $Date: July 6, 2009 17:25:36 $
//###########################################################################
//
// FILE: F28027.cmd
//
// TITLE: Linker Command File For F28027 Device
//
//###########################################################################
// $TI Release: 2802x C/C++ Header Files and Peripheral Examples V1.29 $
// $Release Date: January 11, 2011 $
//###########################################################################
*/

/* ======================================================
// For Code Composer Studio V2.2 and later
// ---------------------------------------
// In addition to this memory linker command file,
// add the header linker command file directly to the project.
// The header linker command file is required to link the
// peripheral structures to the proper locations within
// the memory map.
//
// The header linker files are found in <base>\DSP2802_Headers\cmd
//
// For BIOS applications add: DSP2802x_Headers_BIOS.cmd
// For nonBIOS applications add: DSP2802x_Headers_nonBIOS.cmd
========================================================= */

/* ======================================================
// For Code Composer Studio prior to V2.2
// --------------------------------------
// 1) Use one of the following -l statements to include the
// header linker command file in the project. The header linker
// file is required to link the peripheral structures to the proper
// locations within the memory map */

/* Uncomment this line to include file only for non-BIOS applications */
/* -l DSP2802x_Headers_nonBIOS.cmd */

/* Uncomment this line to include file only for BIOS applications */
/* -l DSP2802x_Headers_BIOS.cmd */

/* 2) In your project add the path to <base>\DSP2802x_headers\cmd to the
library search path under project->build options, linker tab,
library search path (-i).
/*========================================================= */

/* Define the memory block start/length for the F28027
PAGE 0 will be used to organize program sections
PAGE 1 will be used to organize data sections

Notes:
Memory blocks on F2802x are uniform (ie same
physical memory) in both PAGE 0 and PAGE 1.
That is the same memory region should not be
defined for both PAGE 0 and PAGE 1.
Doing so will result in corruption of program
and/or data.

The L0 memory block is mirrored - that is
it can be accessed in high memory or low memory.
For simplicity only one instance is used in this
linker file.

Contiguous SARAM memory blocks or flash sectors can be
be combined if required to create a larger memory block.
*/

MEMORY
{
PAGE 0: /* Program Memory */
/* Memory (RAM/FLASH/OTP) blocks can be moved to PAGE1 for data allocation */

OTP : origin = 0x3D7800, length = 0x000400 /* on-chip OTP */

FLASHA_C : origin = 0x3F2000, length = 0x005F80 /* on-chip FLASH A, B and C */
CSM_RSVD : origin = 0x3F7F80, length = 0x000076 /* Part of FLASHA. Program with all 0x0000 when CSM is in use. */
BEGIN : origin = 0x3F7FF6, length = 0x000002 /* Part of FLASHA. Used for "boot to Flash" bootloader mode. */
CSM_PWL_P0 : origin = 0x3F7FF8, length = 0x000008 /* Part of FLASHA. CSM password locations in FLASHA */

IQTABLES : origin = 0x3FE000, length = 0x000B50 /* IQ Math Tables in Boot ROM */
IQTABLES2 : origin = 0x3FEB50, length = 0x00008C /* IQ Math Tables in Boot ROM */
IQTABLES3 : origin = 0x3FEBDC, length = 0x0000AA /* IQ Math Tables in Boot ROM */

ROM : origin = 0x3FF27C, length = 0x000D44 /* Boot ROM */
RESET : origin = 0x3FFFC0, length = 0x000002 /* part of boot ROM */
VECTORS : origin = 0x3FFFC2, length = 0x00003E /* part of boot ROM */

P_DRAML0 : origin = 0x008000, length = 0x001000 /* on-chip PRAM and DRAM blocks L0 */


PAGE 1 : /* Data Memory */
/* Memory (RAM/FLASH/OTP) blocks can be moved to PAGE0 for program allocation */
/* Registers remain on PAGE1 */

RAMM0_M1 : origin = 0x000000, length = 0x000800 /* on-chip RAM block M0 + M1 */
FLASHD : origin = 0x3F0000, length = 0x002000 /* on-chip FLASH */

}

/* Allocate sections to memory blocks.
Note:
codestart user defined section in DSP28_CodeStartBranch.asm used to redirect code
execution when booting to flash
ramfuncs user defined section to store functions that will be copied from Flash into RAM
*/

SECTIONS
{

/*Flash28_API:
{
-lFlash2802x_API_V201.lib(.text)
-lFlash2802x_API_V201.lib(.econst)
} LOAD = FLASHD,
RUN = PRAML0,
LOAD_START(_Flash28_API_LoadStart),
LOAD_END(_Flash28_API_LoadEnd),
RUN_START(_Flash28_API_RunStart),
PAGE = 0*/

/* Allocate uninitalized data sections: */
.stack : > RAMM0_M1 PAGE = 1
.ebss : > P_DRAML0 PAGE = 0
.esysmem : > RAMM0_M1 PAGE = 1
.params : > FLASHD PAGE = 1
/*
FASTlib_public : load = FLASHA_D PAGE = 0
{
-lfast_public.lib(.econst)
-lfast_public.lib(.text)
}
*/
//userfuncs : > RAMUSER PAGE = 0

//, crc_table(_flashAD_CRCtable)
/* Allocate program areas: */
.cinit : > FLASHA_C PAGE = 0
.pinit : > FLASHA_C PAGE = 0
.text : > FLASHA_C PAGE = 0
codestart : > BEGIN PAGE = 0
ramfuncs : LOAD = FLASHA_C,PAGE = 0
RUN = P_DRAML0,PAGE = 0
LOAD_START(_RamfuncsLoadStart),
LOAD_END(_RamfuncsLoadEnd),
RUN_START(_RamfuncsRunStart)


csmpasswds : > CSM_PWL_P0 PAGE = 0
csm_rsvd : > CSM_RSVD PAGE = 0

/* Initalized sections go in Flash */
/* For SDFlash to program these, they must be allocated to page 0 , crc_table(_flashAD_CRCtable)*/
.econst : > FLASHA_C PAGE = 0
.switch : > FLASHA_C PAGE = 0

/* Allocate IQ math areas: */
IQmath : > FLASHA_C PAGE = 0 /* Math Code */


IQmathTables : > IQTABLES, PAGE = 0, TYPE = NOLOAD

/* Uncomment the section below if calling the IQNexp() or IQexp()
functions from the IQMath.lib library in order to utilize the
relevant IQ Math table in Boot ROM (This saves space and Boot ROM
is 1 wait-state). If this section is not uncommented, IQmathTables2
will be loaded into other memory (SARAM, Flash, etc.) and will take
up space, but 0 wait-state is possible.
*/
/*
IQmathTables2 : > IQTABLES2, PAGE = 0, TYPE = NOLOAD
{

IQmath.lib<IQNexpTable.obj> (IQmathTablesRam)

}
*/
/* Uncomment the section below if calling the IQNasin() or IQasin()
functions from the IQMath.lib library in order to utilize the
relevant IQ Math table in Boot ROM (This saves space and Boot ROM
is 1 wait-state). If this section is not uncommented, IQmathTables2
will be loaded into other memory (SARAM, Flash, etc.) and will take
up space, but 0 wait-state is possible.
*/
/*
IQmathTables3 : > IQTABLES3, PAGE = 0, TYPE = NOLOAD
{

IQmath.lib<IQNasinTable.obj> (IQmathTablesRam)

}
*/

/* .reset is a standard section used by the compiler. It contains the */
/* the address of the start of _c_int00 for C Code. /*
/* When using the boot ROM this section and the CPU vector */
/* table is not needed. Thus the default type is set here to */
/* DSECT */
.reset : > RESET, PAGE = 0, TYPE = DSECT
vectors : > VECTORS PAGE = 0, TYPE = DSECT

}

/*
//===========================================================================
// End of file.
//===========================================================================
*/

 

  • Hi James,

    F28034 does not a instaspin part ie -F. You can try the F28035.cmd file present here:
    C:\ti\controlSUITE\device_support\f2803x\v130\DSP2803x_common\cmd

    Also, migration should be easy enough until you're not using instaspin based motor library .

    Regards,
    Gautam
  • I actually noticed that there is a F28034.cmd in the directory you mention.   I did a file compare with the F28035.cmd in the directory you mention.  Since they appear to be the same I decided to take the  F28034.cmd file and modify as I have posted at the bottom of this post.   This is so my code is placed the same way as it is for the 28027.   It doesn't seem to matter which cmd file I use.  I get the following problem.  When the following code gets executed the 28034 seems to get reset in the debugger.

    //////////////////////////////////////////////////////////////////////////////////////

    void HAL_setParams(HAL_Handle handle, const USER_Params *pUserParams)

    {
    uint_least8_t cnt;
    HAL_Obj *obj = (HAL_Obj *) handle;
    _iq beta_lp_pu = _IQ(pUserParams->offsetPole_rps / (float_t )pUserParams->ctrlFreq_Hz);

    ///////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////

    Why would the _IQ method cause a reset?

    If I single step into the method using the debugger it executes these two statements

    626 _iq beta_lp_pu = _IQ(
    3f272b: D05C MOVB XAR0, #0x5c
    623 void HAL_setParams(HAL_Handle handle, const USER_Params *pUserParams) {
    3f272c: 8BA4 MOVL XAR1, @XAR4

    Single stepping again seems to jump past this statement

    3f272d:   A04E        MOVL         *-SP[14], XAR5

    and end up at this statement

    3f272e:   0693        MOVL         ACC, *+XAR3[AR0]

    When I single step again the 28034 resets.

    It seems the _IQ function above is in IQmath.lib.   I have a IQmath.lib in my project directory.

    I was able to find an IQmath.lib in theses directories that is the same as the one in my project directory when I do a file compare. 

    C:\ti\controlSUITE\libs\math\IQmath\v15b\lib

    C:\ti\controlSUITE\libs\math\IQmath\v15c\lib

    Can I expect to use the same IQmath.lib for the 28034?

    Why would the code above cause the 28034 to reset?

    /*
    //###########################################################################
    //
    // FILE: F28034.cmd
    //
    // TITLE: Linker Command File For F28034 Device
    //
    //###########################################################################
    // $TI Release: F2803x C/C++ Header Files and Peripheral Examples V130 $
    // $Release Date: May 8, 2015 $
    // $Copyright: Copyright (C) 2009-2015 Texas Instruments Incorporated -
    // http://www.ti.com/ ALL RIGHTS RESERVED $
    //###########################################################################
    */

    /* ======================================================
    // For Code Composer Studio V2.2 and later
    // ---------------------------------------
    // In addition to this memory linker command file,
    // add the header linker command file directly to the project.
    // The header linker command file is required to link the
    // peripheral structures to the proper locations within
    // the memory map.
    //
    // The header linker files are found in <base>\DSP2803x_Headers\cmd
    //
    // For BIOS applications add: DSP2803x_Headers_BIOS.cmd
    // For nonBIOS applications add: DSP2803x_Headers_nonBIOS.cmd
    ========================================================= */

    /* ======================================================
    // For Code Composer Studio prior to V2.2
    // --------------------------------------
    // 1) Use one of the following -l statements to include the
    // header linker command file in the project. The header linker
    // file is required to link the peripheral structures to the proper
    // locations within the memory map */

    /* Uncomment this line to include file only for non-BIOS applications */
    /* -l DSP2803x_Headers_nonBIOS.cmd */

    /* Uncomment this line to include file only for BIOS applications */
    /* -l DSP2803x_Headers_BIOS.cmd */

    /* 2) In your project add the path to <base>\DSP2803x_headers\cmd to the
    library search path under project->build options, linker tab,
    library search path (-i).
    /*========================================================= */

    /* Define the memory block start/length for the F28034
    PAGE 0 will be used to organize program sections
    PAGE 1 will be used to organize data sections

    Notes:
    Memory blocks on F2803x are uniform (ie same
    physical memory) in both PAGE 0 and PAGE 1.
    That is the same memory region should not be
    defined for both PAGE 0 and PAGE 1.
    Doing so will result in corruption of program
    and/or data.

    L0 memory block is mirrored - that is
    it can be accessed in high memory or low memory.
    For simplicity only one instance is used in this
    linker file.

    Contiguous SARAM memory blocks or flash sectors can be
    be combined if required to create a larger memory block.
    */

    MEMORY
    {
    PAGE 0: /* Program Memory */
    /* Memory (RAM/FLASH/OTP) blocks can be moved to PAGE1 for data allocation */
    OTP : origin = 0x3D7800, length = 0x000400 /* on-chip OTP */
    FLASHH : origin = 0x3E8000, length = 0x002000 /* on-chip FLASH */
    FLASHG : origin = 0x3EA000, length = 0x002000 /* on-chip FLASH */
    FLASHF : origin = 0x3EC000, length = 0x002000 /* on-chip FLASH */
    FLASHE : origin = 0x3EE000, length = 0x002000 /* on-chip FLASH */
    FLASHA_C : origin = 0x3F2000, length = 0x005F80 /* on-chip FLASH A, B and C */

    CSM_RSVD : origin = 0x3F7F80, length = 0x000076 /* Part of FLASHA. Program with all 0x0000 when CSM is in use. */
    BEGIN : origin = 0x3F7FF6, length = 0x000002 /* Part of FLASHA. Used for "boot to Flash" bootloader mode. */
    CSM_PWL_P0 : origin = 0x3F7FF8, length = 0x000008 /* Part of FLASHA. CSM password locations in FLASHA */

    IQTABLES : origin = 0x3FE000, length = 0x000B50 /* IQ Math Tables in Boot ROM */
    IQTABLES2 : origin = 0x3FEB50, length = 0x00008C /* IQ Math Tables in Boot ROM */
    IQTABLES3 : origin = 0x3FEBDC, length = 0x0000AA /* IQ Math Tables in Boot ROM */

    ROM : origin = 0x3FF27C, length = 0x000D44 /* Boot ROM */
    RESET : origin = 0x3FFFC0, length = 0x000002 /* part of boot ROM */
    VECTORS : origin = 0x3FFFC2, length = 0x00003E /* part of boot ROM */
    P_DRAML0 : origin = 0x008000, length = 0x001000 /* on-chip PRAM and DRAM blocks L0 */


    PAGE 1 : /* Data Memory */
    /* Memory (RAM/FLASH/OTP) blocks can be moved to PAGE0 for program allocation */
    /* Registers remain on PAGE1 */

    BOOT_RSVD : origin = 0x000000, length = 0x000050 /* Part of M0, BOOT rom will use this for stack */
    RAMM0_M1 : origin = 0x000050, length = 0x0007B0 /* on-chip RAM block M0 + M1 */
    FLASHD : origin = 0x3F0000, length = 0x002000 /* on-chip FLASH */


    }

    /* Allocate sections to memory blocks.
    Note:
    codestart user defined section in DSP28_CodeStartBranch.asm used to redirect code
    execution when booting to flash
    ramfuncs user defined section to store functions that will be copied from Flash into RAM
    */

    SECTIONS
    {

    /* Allocate program areas: */
    .cinit : > FLASHA_C PAGE = 0
    .pinit : > FLASHA_C PAGE = 0
    .text : > FLASHA_C PAGE = 0
    codestart : > BEGIN PAGE = 0
    ramfuncs : LOAD = FLASHA_C,PAGE = 0
    RUN = P_DRAML0,PAGE = 0
    LOAD_START(_RamfuncsLoadStart),
    LOAD_SIZE(_RamfuncsLoadEnd),
    RUN_START(_RamfuncsRunStart)

    csmpasswds : > CSM_PWL_P0 PAGE = 0
    csm_rsvd : > CSM_RSVD PAGE = 0

    /* Allocate uninitalized data sections: */
    .stack : > RAMM0_M1 PAGE = 1
    .ebss : > P_DRAML0 PAGE = 0
    .esysmem : > RAMM0_M1 PAGE = 1
    .params : > FLASHD PAGE = 1

    /* Initalized sections go in Flash */
    /* For SDFlash to program these, they must be allocated to page 0 */
    .econst : > FLASHA_C PAGE = 0
    .switch : > FLASHA_C PAGE = 0

    /* Allocate IQ math areas: */
    IQmath : > FLASHA_C PAGE = 0 /* Math Code */
    IQmathTables : > IQTABLES, PAGE = 0, TYPE = NOLOAD

    /* Uncomment the section below if calling the IQNexp() or IQexp()
    functions from the IQMath.lib library in order to utilize the
    relevant IQ Math table in Boot ROM (This saves space and Boot ROM
    is 1 wait-state). If this section is not uncommented, IQmathTables2
    will be loaded into other memory (SARAM, Flash, etc.) and will take
    up space, but 0 wait-state is possible.
    */
    /*
    IQmathTables2 : > IQTABLES2, PAGE = 0, TYPE = NOLOAD
    {

    IQmath.lib<IQNexpTable.obj> (IQmathTablesRam)

    }
    */
    /* Uncomment the section below if calling the IQNasin() or IQasin()
    functions from the IQMath.lib library in order to utilize the
    relevant IQ Math table in Boot ROM (This saves space and Boot ROM
    is 1 wait-state). If this section is not uncommented, IQmathTables2
    will be loaded into other memory (SARAM, Flash, etc.) and will take
    up space, but 0 wait-state is possible.
    */
    /*
    IQmathTables3 : > IQTABLES3, PAGE = 0, TYPE = NOLOAD
    {

    IQmath.lib<IQNasinTable.obj> (IQmathTablesRam)

    }
    */

    /* .reset is a standard section used by the compiler. It contains the */
    /* the address of the start of _c_int00 for C Code. /*
    /* When using the boot ROM this section and the CPU vector */
    /* table is not needed. Thus the default type is set here to */
    /* DSECT */
    .reset : > RESET, PAGE = 0, TYPE = DSECT
    vectors : > VECTORS PAGE = 0, TYPE = DSECT

    }

    /*
    //===========================================================================
    // End of file.
    //===========================================================================
    */