This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

duplicate section name

I recently converted a CC3.3 project into CCS6. Without importing I created a new project and add the required files and built the project. It was successful. Got the warning build attribute vendor section TI missing Flash2811_API_V210.lib. I ignored it and continued to create the hex file.

I used the

 "${CG_TOOL_HEX}" -i "${BuildArtifactFileName}" -o "${BuildArtifactFileBaseName}.hex" -order MS -romwidth 16

command to generate the hex

after generating the hex. I got a warning

duplicate section name test3.out(SciaRegsFile) (ignored) test3 

what is the cause for this warning