Other Parts Discussed in Thread: CONTROLSUITE
Hi,
Can any one help me for BLDC motor control Algorithm.
after installation of controlSUITE. I got modules for sensorless BLDC control Algorithm
C:\TI\controlSUITE\libs\app_libs\motor_control\math_blocks\fixed
C:\TI\controlSUITE\libs\app_libs\motor_control\drivers\f2803x
by using this module. i have succufully commutate the sensorless BLDC motor
and used in my application. it ran good. i have rn BLDC sensolress motor with 3600 RPM
but i have facing problem at start of the motor.
1) RC3_MACRO module
2) IMPULSE_MACRO module
above module used for start up commutation of sensorless BLDC motor. when i started motor was taking 10A to 20A
phase current.when it reaches at ramp level i switched in to Actual phase voltage feedback & close the system.
after that it tooks 1A current which is correct as per my load.
so i didin't understand why BLDC motor tooks high current @ start up?