Other Parts Discussed in Thread: LAUNCHXL-F28069M, DRV8301, BOOSTXL-DRV8301
Hi,
I am trying to use the BOOSTXL-DRV8301 with a LAUNCHXL-F28069M to create a SPI communication with DRV8301 and a temperature IC (ADT7310). At the moment I am trying to figure out how to modify the "proj_lab03c" project in order to control a motor while receiving information from the ADT7310. The ADT7310 and the DRV8301 will be on the same SPI (SPIB).
After spending a bit of time trying to find in the code where the Chip Select GPIO is driven low or high to enable the communication with the DRV8301, I still can not find it.
Can you help me to understand why?
Regards,