Hello,
I work with a F28035.
I wonder if I can safely define a memory allocation over multiple physical memories.
I mean that in my memory mapping file I have:
PAGE 1 : BOOT_RSVD : origin = 0x000000, length = 0x000050 /* Part of M0, BOOT rom will use this for stack */ RAM_M0PART2_M1 : origin = 0x000050, length = 0x0007B0
Memory allocation RAM_M0PART2_M1 may be used for any section depending on my application.
I wonder what would happen if the a variable is defined a the boundary of both memories.
So my questions :
- Can I used RAM_M0PART2_M1 without any special care for all kinds of sections?
- If not, which sections need special care?
- Where can I find a document explaining this behavior?
Thank you!