This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi all,
I have made a customised Card using the F28335. Although my emulator is getting connected to the device. The issue with the card is that I am unable to dump the code into the RAM using the emulator. I have observed the Reset signal /XRS & On Card Oscillator to be Ok. Below I am sharing the part number of the device & the Console Error Report generated by CCS ver5.3.
FULL PART NUMBER IS TMS320F28335PGFA CA-36A7ZYW G4.
CONSOLE ERROR REPORT:
C28x: Flash programmer: warning: The configured device(TMS320F28335), does not match the detected device.
GEL Output:
ADC calibration not complete. check if the device is unlocked and recalibrate.
Trouble setting the Breakpoint with the action "Finish Auto Run" at 0x99f8:(Error-1066 @ 0x99F8) .Unable to set the required breakpoint in memory. Verify that the breakpoint address is in writable memory.(Emulation package 5.0.471.0)
Can't run target CPU:(Error -1041 @ 0x97CF) The emulator reported an error.
Failed Software Reset:(Error -1140 @ 0x0) Lost debug connection to the device. Reset the device and retry operation.
Kindly help to Resolve the issue @ the earliest.
Regards
Shijesh