This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Delfino C28335 Experimenter's Kit - Issue with Example Code

Hello, 

I am running the example program "Example_2833xDMA_xintf_to_ram" on the C28335 Experimenter's Kit using CCS 6.0 MCU Ed with a XDS100v2. 

Specifically, I am having issues with DMAbuf2 (in Zone 7 connected to the SRAM). When data is written into DMSbuf2. it writes FFFF to all elements in the array (I have checked it in memory viewer)  but its suppose to write 0-1024. 

What could be the reason for this and why im not getting the required results.