Dear all,
Actually, i am working with eZdsp F28335 but i have a problem with reading ADC. I have already connected ADCLO to GND, i used internal reference but i can not find ADCREFIN on the card (for connecting to GND). Otherwise, when i change the input voltage of ADC from 0 to 3 volt, it work with the range 0 - 700 mV,. (I used a multimetter to see the change of voltage), so when the voltage is 1 Volt for exemple, the voltage of the ADC input is around 800mV (there are consomable), but from 0 to 700mV, it is same.
Please help me to explain why the ADC work when the input is from 0 to 700mV (in the data sheet say from 0 to 3V), maybe cause of do not connect ADCREFIN to GND?
Many thanks
Dang-Thanh