Good Day.
We are using the c28m35h52c1 controller and the CCS v.6.1.3 and found out that the usb_dev_serial driver from windows_drivers directory does not work on Windows 10.
First, OS does not allow to install the driver.
Second. If we use a workaround the driver is installed and looks like successfully functioining in Control Panel. But actually, the driver does not work - if we try to open the port the system returns the error.
Final note. We can install the dirver on Windows 7 and it continues working after updating the OS to Windows 10.