Other Parts Discussed in Thread: BOOSTXL-DRV8301
I bought the LaunchXL- F28027F and BoostXL-DRV8301 to use in a small rotating test fixture. Using CCS 6.1.2 I've been able to work through the labs up to 5b, and even with a $12 hobby motor (USER_MOTOR_Rs = 0.072, USER_MOTOR_Ls_d = 6.0e-06, USER_MOTOR_RATED_FLUX = 0.0038) I'm getting better results than with the brushed motor & simple PWM controller it replaced. When I try Lab 9, the motor still runs fine but the variable gMotorVars.Vs never changes from 0.0, nor do Vd, Vq, Id_A, Iq_A, or Is_A. I've set gMotorVars.Flag_enableFieldWeakening to 1, is there something else that I've missed for this lab?