Other Parts Discussed in Thread: INSTASPIN-BLDC, DRV8301, CONTROLSUITE
Hi All,
I purchase DRV8301-HC- EVM Rev D board (Serial No D1A_1512079), I am able to control the Board through the InstaSpin GUI, but now i want to perform the same operation though my Host micro-controller, How do i do that. Please clarify my below question as well.
1) What is the default program/project flashed on the PICOLO controller.
2) I need to develop an USART Rapper on PICOLO, on which project should I do that, to establish communication between the Host controller and PICOLO.
3) In case you have any working code please share. I should be able to control the BLDC through Hyper terminal, later which i can replace with my Host controller. I am ok even if it is SPI based master slave communication.
Regards
Mahesh Prasath.