This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Digital Control Design and Implementation of a DSP Based High-Frequency DC-DC Switching Power Converter by Shamim

 

Dear Shamim,

I came across your paper entitled; (see attached)

“Digital Control Design and Implementation of a DSP Based High-Frequency DC-DC Switching Power Converter”

Very good paper and reference ; however how do you get equations Gp and Gc; I need actual equations in terms of general circuit parameters (R’s ,L and C’s ect) ; also can you please send me MATLAB .m  scrip file you used to plot all the figures in the paper. Do you have the C++ code to download for this paper  as a reference for my design.

I am planning to use the TMS320F DSP to implement digital multiphase DC-DC ,you have any app notes on multiphase CPU type DC-DC application you can share with me please. (12VDC to 0.7-1.3VDC , 200 Amp 6ph interleaved Buck as per Intel VRM 12.5/13 spec )

I appreciate your help and support , do you have a phone number I can call you if I need some more help in implementation ,

 Thank you,

Ivan Vuk

Intel

Chandler, AZ