Other Parts Discussed in Thread: BOOST-DRV8711, TMS320F28377S, DRV8711
I will start out by saying I am new to SPI.
I am attemting to use the TMS320F28377S Launchpad with the BOOST-DRV8711.
My problem is when I write out the register data from the TMS320F28377S using the SPI everything looks good, the issue comes in to play when I try and read the register back I get all 1's
I am attempting to write out all 16-bits at onetime and read all 16-bits at one time.
Below is my code.
Any help would be greatly appreciated.
//###########################################################################
// Main Program
//###########################################################################
#include "F28x_Project.h" // Device Headerfile and Examples Include File
#include "DRV8711.h" // Motor Driver Headerfile
#include "mySPI.h" // SPI Headerfile
#include "myGPIO.h" // GPIO and Communication Headerfile
void main(void)
{
// Step 1. Initialize System Control:
// PLL, WatchDog, enable Peripheral Clocks
InitSysCtrl();
// Step 2. Initialize GPIO:
initmyGPIO();
// Step 3. Clear all __interrupts and initialize PIE vector table:
// Disable CPU __interrupts
DINT;
// Initialize PIE control registers to their default state.
InitPieCtrl();
// Disable CPU __interrupts and clear all CPU __interrupt flags:
IER = 0x0000;
IFR = 0x0000;
// Initialize the PIE vector table with pointers to the shell Interrupt
// Service Routines (ISR).
InitPieVectTable();
// Step 4. Initialize the Device Peripherals:
initmySPI(); // init SPI
// Step 5. User specific code:
initDRV8711(); // Form Motor Driver Registers
WriteAllRegisters(); // Write Motor Driver Registers
ReadAllRegisters(); // Read Motor Driver Registers
}
/*******************************************************************************************
FILE: myGpio.c
TITLE: Device GPIO Setup
*******************************************************************************************/
#include "F2837xS_device.h" // F2837xS Headerfile Include File
#include "F2837xS_Examples.h" // F2837xS Examples Include File
/* Initialize GPIO and Communication Pins */
void initmyGPIO(void)
{
// Enable GPIO outputs 4, 41-43, 61-62, and 78
GpioCtrlRegs.GPAPUD.bit.GPIO4 = 0; // Enable pullup on GPIO4
GpioDataRegs.GPASET.bit.GPIO4 = 1; // Load output latch
GpioCtrlRegs.GPAMUX1.bit.GPIO4 = 0; // GPIO4 = GPIO4
GpioCtrlRegs.GPADIR.bit.GPIO4 = 1; // GPIO4 = output
GpioCtrlRegs.GPBPUD.bit.GPIO41 = 0; // Enable pullup on GPIO42 G_nSLEEP = low
GpioDataRegs.GPBSET.bit.GPIO41 = 1; // Load output latch
GpioCtrlRegs.GPBMUX1.bit.GPIO41 = 0; // GPIO41 = GPIO41
GpioCtrlRegs.GPBDIR.bit.GPIO41 = 1; // GPIO41 = output
GpioCtrlRegs.GPBPUD.bit.GPIO42 = 0; // Enable pullup on GPIO42 G_DIR_AIN2 = low
GpioDataRegs.GPBSET.bit.GPIO42 = 1; // Load output latch
GpioCtrlRegs.GPBMUX1.bit.GPIO42 = 0; // GPIO42 = GPIO42
GpioCtrlRegs.GPBDIR.bit.GPIO42 = 1; // GPIO42 = output
GpioCtrlRegs.GPBPUD.bit.GPIO43 = 0; // Enable pullup on GPIO42 G_DIR_AIN2 = low
GpioDataRegs.GPBSET.bit.GPIO43 = 1; // Load output latch
GpioCtrlRegs.GPBMUX1.bit.GPIO43 = 0; // GPIO43 = GPIO43
GpioCtrlRegs.GPBDIR.bit.GPIO43 = 1; // GPIO43 = output
GpioCtrlRegs.GPBPUD.bit.GPIO61 = 0; // Enable GPIO61 as G_RESET = low
GpioDataRegs.GPBSET.bit.GPIO61 = 1; // Load output latch
GpioCtrlRegs.GPBMUX2.bit.GPIO61 = 0; // GPIO61 = GPIO61
GpioCtrlRegs.GPBDIR.bit.GPIO61 = 1; // GPIO61 = output
GpioCtrlRegs.GPBPUD.bit.GPIO62 = 0; // Enable GPIO62 as G_RESET = low
GpioDataRegs.GPBSET.bit.GPIO62 = 1; // Load output latch
GpioCtrlRegs.GPBMUX2.bit.GPIO62 = 0; // GPIO62 = GPIO62
GpioCtrlRegs.GPBDIR.bit.GPIO62 = 1; // GPIO62 = output
GpioCtrlRegs.GPCPUD.bit.GPIO78 = 0; // Enable GPIO78 as (SPISTEA)
GpioDataRegs.GPCSET.bit.GPIO78 = 1; // Load output latch
GpioCtrlRegs.GPCMUX1.bit.GPIO78 = 0; // GPI78 = GPIO78
GpioCtrlRegs.GPCDIR.bit.GPIO78 = 1; // GPIO78 = output
// Enable SPI-A on GPIO58 - GPIO60
/* Enable internal pull-up for the selected pins */
GpioCtrlRegs.GPBPUD.bit.GPIO58 = 0; // Enable pull-up on GPIO58 (SPISIMOA)
GpioCtrlRegs.GPBPUD.bit.GPIO59 = 0; // Enable pull-up on GPIO59 (SPISOMIA)
GpioCtrlRegs.GPBPUD.bit.GPIO60 = 0; // Enable pull-up on GPIO60 (SPICLKA)
/* Set qualification for selected pins to Asynch only */
GpioCtrlRegs.GPBQSEL2.bit.GPIO58 = 3; // GPIO58 (SPISIMOA)
GpioCtrlRegs.GPBQSEL2.bit.GPIO59 = 3; // GPIO59 (SPISOMIA)
GpioCtrlRegs.GPBQSEL2.bit.GPIO60 = 3; // GPIO60 (SPICLKA)
/* Configure SPI-A pins using GPIO regs */
GpioCtrlRegs.GPBMUX2.bit.GPIO58 = 1; // Configure as SPISIMOA
GpioCtrlRegs.GPBMUX2.bit.GPIO59 = 1; // Configure as SPISOMIA
GpioCtrlRegs.GPBMUX2.bit.GPIO60 = 1; // Configure as SPICLKA
EDIS;
}
/*****************************************************************************/
// Function to setup variables for the DRV8711 Control register and set initial pin state
void initDRV8711()
{
// Set Default GPIO Settings
GpioDataRegs.GPCCLEAR.bit.GPIO78 = 1; // SPIA_CS = low;
GpioDataRegs.GPBCLEAR.bit.GPIO41 = 1; // G_nSLEEP = low;
GpioDataRegs.GPBCLEAR.bit.GPIO61 = 1; // G_RESET = low;
GpioDataRegs.GPBCLEAR.bit.GPIO43 = 1; // G_STEP_AIN1 = low;
GpioDataRegs.GPBCLEAR.bit.GPIO42 = 1; // G_DIR_AIN2 = low;
GpioDataRegs.GPBSET.bit.GPIO62 = 1; // G_nFAULT = high;
GpioDataRegs.GPASET.bit.GPIO4 = 1; // G_nSTALL = high;
// Set Default Register Settings
// CTRL Register
G_CTRL_REG.Address = 0x00; // CRTL Register Address
G_CTRL_REG.DTIME = 0x03; // 850ns
G_CTRL_REG.ISGAIN = 0x01; // Gain of 10
G_CTRL_REG.EXSTALL = 0x00; // Internal Stall Detect
G_CTRL_REG.MODE = 0x00; // Full Step
G_CTRL_REG.RSTEP = 0x01; // Step No Action
G_CTRL_REG.RDIR = 0x00; // Direction set by DIR Pin
G_CTRL_REG.ENBL = 0x01; // Enable motor
// 0000 1101 0000 0001
}
/*************************************************************************************/
// Function to construct 16 bit value to write to DRV8711 register
void WriteAllRegisters()
{
Uint16 REGWRITE = 0x000; // Set MSB to 0 for write
unsigned char sdata = 0x000; // send data
// Write CTRL Register
sdata = REGWRITE | (G_CTRL_REG.Address << 12) | (G_CTRL_REG.DTIME << 10) |
(G_CTRL_REG.ISGAIN << 8) | (G_CTRL_REG.EXSTALL << 7) | (G_CTRL_REG.MODE << 3) |
(G_CTRL_REG.RSTEP << 2) | (G_CTRL_REG.RDIR << 1) | (G_CTRL_REG.ENBL);
SPI_DRV8711_ReadWrite(sdata); // Go to function write SPI data
}
/************************************************************************************/
// Function to read 16 bit register value from DRV8711
void ReadAllRegisters()
{
Uint16 REGREAD = 0x8000; // Set MSB to 1 for read
Uint16 rdata = 0x0000; // receive data
unsigned char sdata = 0x0000; // send data
// Read CTRL Register
sdata = REGREAD | (G_CTRL_REG.Address << 12);
rdata = SPI_DRV8711_ReadWrite(sdata); // Go to SPI function read DRV8711 register
G_CTRL_REG.DTIME = ((rdata >> 10) & 0x03);
G_CTRL_REG.ISGAIN = ((rdata >> 8) & 0x03);
G_CTRL_REG.EXSTALL = ((rdata >> 7) & 0x01);
G_CTRL_REG.MODE = ((rdata >> 3) & 0x0F);
G_CTRL_REG.RSTEP = ((rdata >> 2) & 0x01);
G_CTRL_REG.RDIR = ((rdata >> 1) & 0x01);
G_CTRL_REG.ENBL = ((rdata >> 0) & 0x01);
}
/************************************************************************************/
// Function to setup SPI for communication
void initmySPI()
{
EALLOW;
SpiaRegs.SPICCR.bit.SPISWRESET = 0; // SPI software reset
SpiaRegs.SPIBRR.all = 0x007F; // SPI Baud Rate Control. 1.5Mhz
SpiaRegs.SPICCR.all = 0x000F; // Reset on, rising edge, 16-bit
SpiaRegs.SPICTL.all = 0x0006; // Enable master mode, normal phase, enable talk, and SPI int disabled.
SpiaRegs.SPIBRR.all = 0x007F; // SPI Baud Rate Control. 1.5Mhz
SpiaRegs.SPICCR.all = 0x008F; // Relinquish SPI from Reset No loop back
SpiaRegs.SPIPRI.bit.FREE = 1; // Set so breakpoints don't disturb xmission
EDIS;
}
Uint16 SPI_DRV8711_ReadWrite(unsigned char sdata)
{
Uint16 rdata = 0x000;
GpioDataRegs.GPCSET.bit.GPIO78 = 1; // Selects the DRV8711
SpiaRegs.SPITXBUF = sdata; // Transmit Buffer
while (SpiaRegs.SPISTS.bit.INT_FLAG != 1) {} // Wait until character has been transferred
rdata |= SpiaRegs.SPIRXBUF; // Receive Buffer
GpioDataRegs.GPCCLEAR.bit.GPIO78 = 1; // Releases the DRV8711
return rdata;
}
Thanks again for any help you can give me.