Other Parts Discussed in Thread: TMS320F28335, CONTROLSUITE
Hello everybody,
I am working with TMS320F28335 eZDSP from Spectrum Digital.
I have a problem about reading values from ADCIN pins from the development board.I use ADCINA0,ADCINA1,ADCIN2,ADCIN3,ADCIN4,ADCIN5,ADCIN6 pins.
I read all the channels as 0 with this code..
Here is the code ;
void main(void)
{
// Step 1. Initialize System Control:
// PLL, WatchDog, enable Peripheral Clocks
// This example function is found in the DSP2833x_SysCtrl.c file.
InitSysCtrl();
EALLOW;
#if (CPU_FRQ_150MHZ) // Default - 150 MHz SYSCLKOUT
#define ADC_MODCLK 0x3 // HSPCLK = SYSCLKOUT/2*ADC_MODCLK2 = 150/(2*3) = 25.0 MHz
#endif
#if (CPU_FRQ_100MHZ)
#define ADC_MODCLK 0x2 // HSPCLK = SYSCLKOUT/2*ADC_MODCLK2 = 100/(2*3) = 12.5 MHz
#endif
EDIS;
// Step 2. Initialize GPIO:
// This example function is found in the DSP2833x_Gpio.c file and
// illustrates how to set the GPIO to it's default state.
EALLOW;
SysCtrlRegs.HISPCP.all = ADC_MODCLK;
EDIS;
InitAdc();
// Configure ADC
AdcRegs.ADCTRL3.bit.SMODE_SEL = 0x1; // Setup simultaneous sampling mode
AdcRegs.ADCMAXCONV.all = 0x0005;
AdcRegs.ADCCHSELSEQ1.bit.CONV00 = 0x0; // Setup conv from ADCINA0 &
AdcRegs.ADCCHSELSEQ1.bit.CONV01 = 0x1; // Setup conv from ADCINA1 &
AdcRegs.ADCCHSELSEQ1.bit.CONV02 = 0x2; // Setup conv from ADCINA2 &
AdcRegs.ADCCHSELSEQ1.bit.CONV03 = 0x3; // Setup conv from ADCINA3 &
AdcRegs.ADCCHSELSEQ2.bit.CONV04 = 0x4; // Setup conv from ADCINA4 &
AdcRegs.ADCCHSELSEQ2.bit.CONV05 = 0x5; // Setup conv from ADCINA5 &
AdcRegs.ADCCHSELSEQ2.bit.CONV06 = 0x6; // Setup conv from ADCINA6 &
for(;;)
{
AdcRegs.ADCTRL2.bit.SOC_SEQ1 = 0X1; // Start of conversion trigger for SEQ1
DELAY_US(1);
adcin0= AdcRegs.ADCRESULT0 ;
adcin1= AdcRegs.ADCRESULT1 ;
adcin2= AdcRegs.ADCRESULT2 ;
adcin3=AdcRegs.ADCRESULT3;
adcin4=AdcRegs.ADCRESULT4;
adcin5=AdcRegs.ADCRESULT5;
adcin6=AdcRegs.ADCRESULT6;
}
ADC.cal.asm
.def _ADC_cal
.asg "0x711C", ADCREFSEL_LOC
;-----------------------------------------------
; _ADC_cal
;-----------------------------------------------
;-----------------------------------------------
; This is the ADC cal routine.This routine is programmed into
; reserved memory by the factory. 0xAAAA and 0xBBBB are place-
; holders for calibration data.
;The actual values programmed by TI are device specific.
;
; This function assumes that the clocks have been
; enabled to the ADC module.
;-----------------------------------------------
.sect ".adc_cal"
_ADC_cal
MOVW DP, #ADCREFSEL_LOC >> 6
MOV @28, #0xAAAA ; actual value may not be 0xAAAA
MOV @29, #0xBBBB ; actual value may not be 0xBBBB
LRETR
ADC.C
#include "DSP2833x_Device.h" // DSP2833x Headerfile Include File
#include "DSP2833x_Examples.h" // DSP2833x Examples Include File
#define ADC_usDELAY 5000L
//---------------------------------------------------------------------------
// InitAdc:
//---------------------------------------------------------------------------
// This function initializes ADC to a known state.
//
void InitAdc(void)
{
extern void DSP28x_usDelay(Uint32 Count);
// *IMPORTANT*
// The ADC_cal function, which copies the ADC calibration values from TI reserved
// OTP into the ADCREFSEL and ADCOFFTRIM registers, occurs automatically in the
// Boot ROM. If the boot ROM code is bypassed during the debug process, the
// following function MUST be called for the ADC to function according
// to specification. The clocks to the ADC MUST be enabled before calling this
// function.
// See the device data manual and/or the ADC Reference
// Manual for more information.
EALLOW;
SysCtrlRegs.PCLKCR0.bit.ADCENCLK = 1;
ADC_cal();
EDIS;
// To powerup the ADC the ADCENCLK bit should be set first to enable
// clocks, followed by powering up the bandgap, reference circuitry, and ADC core.
// Before the first conversion is performed a 5ms delay must be observed
// after power up to give all analog circuits time to power up and settle
// Please note that for the delay function below to operate correctly the
// CPU_RATE define statement in the DSP2833x_Examples.h file must
// contain the correct CPU clock period in nanoseconds.
AdcRegs.ADCTRL3.all = 0x00E0; // Power up bandgap/reference/ADC circuits
DELAY_US(ADC_usDELAY); // Delay before converting ADC channels
// FILE: DSP2833x_Adc.h
//
// TITLE: DSP2833x Device ADC Register Definitions.
//
//###########################################################################
// $TI Release: F2833x/F2823x Header Files and Peripheral Examples V141 $
// $Release Date: November 6, 2015 $
// $Copyright: Copyright (C) 2007-2015 Texas Instruments Incorporated -
// http://www.ti.com/ ALL RIGHTS RESERVED $
//###########################################################################
#ifndef DSP2833x_ADC_H
#define DSP2833x_ADC_H
#ifdef __cplusplus
extern "C" {
#endif
//---------------------------------------------------------------------------
// ADC Individual Register Bit Definitions:
struct ADCTRL1_BITS { // bits description
Uint16 rsvd1:4; // 3:0 reserved
Uint16 SEQ_CASC:1; // 4 Cascaded sequencer mode
Uint16 SEQ_OVRD:1; // 5 Sequencer override
Uint16 CONT_RUN:1; // 6 Continuous run
Uint16 CPS:1; // 7 ADC core clock pre-scalar
Uint16 ACQ_PS:4; // 11:8 Acquisition window size
Uint16 SUSMOD:2; // 13:12 Emulation suspend mode
Uint16 RESET:1; // 14 ADC reset
Uint16 rsvd2:1; // 15 reserved
};
union ADCTRL1_REG {
Uint16 all;
struct ADCTRL1_BITS bit;
};
struct ADCTRL2_BITS { // bits description
Uint16 EPWM_SOCB_SEQ2:1; // 0 EPWM compare B SOC mask for SEQ2
Uint16 rsvd1:1; // 1 reserved
Uint16 INT_MOD_SEQ2:1; // 2 SEQ2 Interrupt mode
Uint16 INT_ENA_SEQ2:1; // 3 SEQ2 Interrupt enable
Uint16 rsvd2:1; // 4 reserved
Uint16 SOC_SEQ2:1; // 5 Start of conversion for SEQ2
Uint16 RST_SEQ2:1; // 6 Reset SEQ2
Uint16 EXT_SOC_SEQ1:1; // 7 External start of conversion for SEQ1
Uint16 EPWM_SOCA_SEQ1:1; // 8 EPWM compare B SOC mask for SEQ1
Uint16 rsvd3:1; // 9 reserved
Uint16 INT_MOD_SEQ1:1; // 10 SEQ1 Interrupt mode
Uint16 INT_ENA_SEQ1:1; // 11 SEQ1 Interrupt enable
Uint16 rsvd4:1; // 12 reserved
Uint16 SOC_SEQ1:1; // 13 Start of conversion trigger for SEQ1
Uint16 RST_SEQ1:1; // 14 Restart sequencer 1
Uint16 EPWM_SOCB_SEQ:1; // 15 EPWM compare B SOC enable
};
union ADCTRL2_REG {
Uint16 all;
struct ADCTRL2_BITS bit;
};
struct ADCASEQSR_BITS { // bits description
Uint16 SEQ1_STATE:4; // 3:0 SEQ1 state
Uint16 SEQ2_STATE:3; // 6:4 SEQ2 state
Uint16 rsvd1:1; // 7 reserved
Uint16 SEQ_CNTR:4; // 11:8 Sequencing counter status
Uint16 rsvd2:4; // 15:12 reserved
};
union ADCASEQSR_REG {
Uint16 all;
struct ADCASEQSR_BITS bit;
};
struct ADCMAXCONV_BITS { // bits description
Uint16 MAX_CONV1:4; // 3:0 Max number of conversions
Uint16 MAX_CONV2:3; // 6:4 Max number of conversions
Uint16 rsvd1:9; // 15:7 reserved
};
union ADCMAXCONV_REG {
Uint16 all;
struct ADCMAXCONV_BITS bit;
};
struct ADCCHSELSEQ1_BITS { // bits description
Uint16 CONV00:4; // 3:0 Conversion selection 00
Uint16 CONV01:4; // 7:4 Conversion selection 01
Uint16 CONV02:4; // 11:8 Conversion selection 02
Uint16 CONV03:4; // 15:12 Conversion selection 03
};
union ADCCHSELSEQ1_REG{
Uint16 all;
struct ADCCHSELSEQ1_BITS bit;
};
struct ADCCHSELSEQ2_BITS { // bits description
Uint16 CONV04:4; // 3:0 Conversion selection 04
Uint16 CONV05:4; // 7:4 Conversion selection 05
Uint16 CONV06:4; // 11:8 Conversion selection 06
Uint16 CONV07:4; // 15:12 Conversion selection 07
};
union ADCCHSELSEQ2_REG{
Uint16 all;
struct ADCCHSELSEQ2_BITS bit;
};
struct ADCCHSELSEQ3_BITS { // bits description
Uint16 CONV08:4; // 3:0 Conversion selection 08
Uint16 CONV09:4; // 7:4 Conversion selection 09
Uint16 CONV10:4; // 11:8 Conversion selection 10
Uint16 CONV11:4; // 15:12 Conversion selection 11
};
union ADCCHSELSEQ3_REG{
Uint16 all;
struct ADCCHSELSEQ3_BITS bit;
};
struct ADCCHSELSEQ4_BITS { // bits description
Uint16 CONV12:4; // 3:0 Conversion selection 12
Uint16 CONV13:4; // 7:4 Conversion selection 13
Uint16 CONV14:4; // 11:8 Conversion selection 14
Uint16 CONV15:4; // 15:12 Conversion selection 15
};
union ADCCHSELSEQ4_REG {
Uint16 all;
struct ADCCHSELSEQ4_BITS bit;
};
struct ADCTRL3_BITS { // bits description
Uint16 SMODE_SEL:1; // 0 Sampling mode select
Uint16 ADCCLKPS:4; // 4:1 ADC core clock divider
Uint16 ADCPWDN:1; // 5 ADC powerdown
Uint16 ADCBGRFDN:2; // 7:6 ADC bandgap/ref power down
Uint16 rsvd1:8; // 15:8 reserved
};
union ADCTRL3_REG {
Uint16 all;
struct ADCTRL3_BITS bit;
};
struct ADCST_BITS { // bits description
Uint16 INT_SEQ1:1; // 0 SEQ1 Interrupt flag
Uint16 INT_SEQ2:1; // 1 SEQ2 Interrupt flag
Uint16 SEQ1_BSY:1; // 2 SEQ1 busy status
Uint16 SEQ2_BSY:1; // 3 SEQ2 busy status
Uint16 INT_SEQ1_CLR:1; // 4 SEQ1 Interrupt clear
Uint16 INT_SEQ2_CLR:1; // 5 SEQ2 Interrupt clear
Uint16 EOS_BUF1:1; // 6 End of sequence buffer1
Uint16 EOS_BUF2:1; // 7 End of sequence buffer2
Uint16 rsvd1:8; // 15:8 reserved
};
union ADCST_REG {
Uint16 all;
struct ADCST_BITS bit;
};
struct ADCREFSEL_BITS { // bits description
Uint16 rsvd1:14; // 13:0 reserved
Uint16 REF_SEL:2; // 15:14 Reference select
};
union ADCREFSEL_REG {
Uint16 all;
struct ADCREFSEL_BITS bit;
};
struct ADCOFFTRIM_BITS{ // bits description
int16 OFFSET_TRIM:9; // 8:0 Offset Trim
Uint16 rsvd1:7; // 15:9 reserved
};
union ADCOFFTRIM_REG{
Uint16 all;
struct ADCOFFTRIM_BITS bit;
};
struct ADC_REGS {
union ADCTRL1_REG ADCTRL1; // ADC Control 1
union ADCTRL2_REG ADCTRL2; // ADC Control 2
union ADCMAXCONV_REG ADCMAXCONV; // Max conversions
union ADCCHSELSEQ1_REG ADCCHSELSEQ1; // Channel select sequencing control 1
union ADCCHSELSEQ2_REG ADCCHSELSEQ2; // Channel select sequencing control 2
union ADCCHSELSEQ3_REG ADCCHSELSEQ3; // Channel select sequencing control 3
union ADCCHSELSEQ4_REG ADCCHSELSEQ4; // Channel select sequencing control 4
union ADCASEQSR_REG ADCASEQSR; // Autosequence status register
Uint16 ADCRESULT0; // Conversion Result Buffer 0
Uint16 ADCRESULT1; // Conversion Result Buffer 1
Uint16 ADCRESULT2; // Conversion Result Buffer 2
Uint16 ADCRESULT3; // Conversion Result Buffer 3
Uint16 ADCRESULT4; // Conversion Result Buffer 4
Uint16 ADCRESULT5; // Conversion Result Buffer 5
Uint16 ADCRESULT6; // Conversion Result Buffer 6
Uint16 ADCRESULT7; // Conversion Result Buffer 7
Uint16 ADCRESULT8; // Conversion Result Buffer 8
Uint16 ADCRESULT9; // Conversion Result Buffer 9
Uint16 ADCRESULT10; // Conversion Result Buffer 10
Uint16 ADCRESULT11; // Conversion Result Buffer 11
Uint16 ADCRESULT12; // Conversion Result Buffer 12
Uint16 ADCRESULT13; // Conversion Result Buffer 13
Uint16 ADCRESULT14; // Conversion Result Buffer 14
Uint16 ADCRESULT15; // Conversion Result Buffer 15
union ADCTRL3_REG ADCTRL3; // ADC Control 3
union ADCST_REG ADCST; // ADC Status Register
Uint16 rsvd1;
Uint16 rsvd2;
union ADCREFSEL_REG ADCREFSEL; // Reference Select Register
union ADCOFFTRIM_REG ADCOFFTRIM; // Offset Trim Register
};
struct ADC_RESULT_MIRROR_REGS
{
Uint16 ADCRESULT0; // Conversion Result Buffer 0
Uint16 ADCRESULT1; // Conversion Result Buffer 1
Uint16 ADCRESULT2; // Conversion Result Buffer 2
Uint16 ADCRESULT3; // Conversion Result Buffer 3
Uint16 ADCRESULT4; // Conversion Result Buffer 4
Uint16 ADCRESULT5; // Conversion Result Buffer 5
Uint16 ADCRESULT6; // Conversion Result Buffer 6
Uint16 ADCRESULT7; // Conversion Result Buffer 7
Uint16 ADCRESULT8; // Conversion Result Buffer 8
Uint16 ADCRESULT9; // Conversion Result Buffer 9
Uint16 ADCRESULT10; // Conversion Result Buffer 10
Uint16 ADCRESULT11; // Conversion Result Buffer 11
Uint16 ADCRESULT12; // Conversion Result Buffer 12
Uint16 ADCRESULT13; // Conversion Result Buffer 13
Uint16 ADCRESULT14; // Conversion Result Buffer 14
Uint16 ADCRESULT15; // Conversion Result Buffer 15
};
//---------------------------------------------------------------------------
// ADC External References & Function Declarations:
//
extern volatile struct ADC_REGS AdcRegs;
extern volatile struct ADC_RESULT_MIRROR_REGS AdcMirror;
#ifdef __cplusplus
}
#endif /* extern "C" */
#endif // end of DSP2833x_ADC_H definition