Hi Everyone,
I am not really sure if I should be posting to this thread, so my apologies in advance.
I am working on an application on which I have to transmit UDP data from a standalone processor to another machine thru a module that uses a USB/IP configuration. The intermediate module is a piece of hardware (proprietary) that encrypts the sent data, and decrypts it before getting to its receiving end. Basically, I do not have to deal with this module much and all I know is that it receives and transmits its data thru USB.
Also, I am familiar with the F28335 processor and I was attempting to use it to transmit UDP data but i realize it does not support this capability.
Would a Ethernet to Serial adapter work for what I am doing? I have seen one on another blog but it has been discontinued. Or would I be better off choosing a processor that supports the UDP protocol?
Any advice is greatly appreciated guys.
Thank you,
Gilmer